Skip to main content
Refused_HC
Associate II
Oct 19, 2026 8:07 AM UTC
Question

White zones on circleProgress

Hello all,

The problem that I’m facing is that two specific zones are showed in white color in my screen. These zones only appear in a circleProgress that is based in an image.

I am using the TouchGFX version 4.26.1, and the MCU is a STM32U575CIUX.

These problem only happens when I save data on the persistent memory of the MCU with this function (source code below):

// Write into flash memory

bool PERSIST_write(RegistroFlash *persist_memory_to_write)

{

uint32_t address = USER_FLASH_START_ADDRESS;

uint8_t *ptr = (uint8_t *)persist_memory_to_write;

FLASH_EraseInitTypeDef erase;

uint32_t pageError;

HAL_StatusTypeDef program_ok_result = HAL_ERROR;

bool function_ok_result = false;



// Unlock the flash memory to write there

HAL_FLASH_Unlock();



// Erase the corresponding flash page (in my case only the last page 255)

// Although we do not use it completely a complete page must be deleted (2 KB)

erase.TypeErase = FLASH_TYPEERASE_PAGES;

erase.Page = (USER_FLASH_START_ADDRESS - FLASH_BASE) / FLASH_PAGE_SIZE;

erase.NbPages = 1;



HAL_FLASHEx_Erase(&erase, &pageError);



// Write the corresponding structure

// The structure RegistroFlash must be multiple of 16 bytes due to the use of FLASH_TYPEPROGRAM_QUADWORD

for (uint32_t i = 0; i < sizeof(RegistroFlash); i += BYTES_PERSIST_BLOCK)

{

program_ok_result = HAL_FLASH_Program(FLASH_TYPEPROGRAM_QUADWORD, address, (uint32_t)(ptr + i));



if (program_ok_result == HAL_OK)

{

address += BYTES_PERSIST_BLOCK;

function_ok_result = true;

}

else

{

function_ok_result = false;

}

}



// Lock the flash memory

HAL_FLASH_Lock();

return (function_ok_result);

}

 

Much thanks in advance to all.

Any other data that is needed just tell me.

 

1 reply

Associate
Oct 19, 2026 8:40 AM UTC

Could you please share a photo of the issue so we can better visualise it? Would you also be able to share the location and method of your frame buffer(s)?