while(state) get stuck for ever !!!
hi
im driving ili9341 lcd with spi1 and w25q128 with spi2 with stm32f103c8t6.
im loading some images from w25q128 to lcd via dma (peripheral to peripheral).
i should check if the last image has been sent to lcd or not before putting other images . so i used :
_Bool LCD_BUSY
before sending new data to lcd i will check it .....
but i get stuck in while loop for ever . and in debugger it says that (_Bool LCD_BUSY ) is 0 !!!
but if i put HAL_DELAY(1); in while loop it will work !
not WORKING:
while(LCD_BUSY){}
working;
while(LCD_BUSY){HAL_DELAY(1);}