Skip to main content
Rostyslav S
Associate II
Oct 17, 2017 1:58 PM UTC
Solved

Which MCU has 3 lane DSI interface

Posted on October 17, 2017 at 15:58

According to

http://www.st.com/content/ccc/resource/technical/document/application_note/group0/1d/b8/33/4f/dc/0a/45/52/DM00287601/files/DM00287601.pdf/jcr:content/translations/en.DM00287601.pdf

, STM32F4 includes DSI interface with up to 2 lanes. See page 15.

I am wondering if there is any MCU with 3 data lanes (L0, L1, L2) and CLK lane?

#stm32f4 #dsi
This topic has been closed for replies.
Nesrine M_O
Nesrine M_OBest answer
Associate
Oct 17, 2017 5:08 PM UTC
Posted on October 17, 2017 at 17:08

Hi

rostokus

,

Unfortunately,there is no STM32 device with 3 DSI data lanes, the STM32 embeded maximum 2 data lanes.

-Nesrine-

3 replies

Nesrine M_O
Associate
Oct 17, 2017 2:16 PM UTC

Posted on October 17, 2017 at 16:16

 Hi rostokus,

The STM32F469/479 devices embeded MIPI® DSI host controller supporting up to 720p 30Hz resolution.

The DSI Host provides a scalable architecture using one or two data lanes.The number of lanes depends on the bandwidth requirements of the application. Each DSI lane has a maximum of 500 Mbit/s data rate, for a total 1Gbit/s rate in dual data lane mode.

Further information are detailed in AN4861application note it may help you.

-Nesrine-

Rostyslav S
Associate II
Oct 17, 2017 4:29 PM UTC
Posted on October 17, 2017 at 16:29

Hi Nesrine,

You said 'using one or two data lanes'.

But my questions is whether you have any MCU with three data lanes?

Recommended app note does not mention about 3 lanes (only two)

Thanks

Nesrine M_O
Nesrine M_OBest answer
Associate
Oct 17, 2017 5:08 PM UTC
Posted on October 17, 2017 at 17:08

Hi

rostokus

,

Unfortunately,there is no STM32 device with 3 DSI data lanes, the STM32 embeded maximum 2 data lanes.

-Nesrine-