Skip to main content
Bing Wang
Associate
Nov 22, 2019 12:28 AM UTC
Question

Whether the TouchGFX can be ported to STM32WB series MCU?

Whether the ToughGFX can be run on the bluetooth SOC STM32WB series MCU? If can where can I find an example?

Thanks and best regards.

This topic has been closed for replies.

2 replies

Martin KJELDSEN
Principal III
Nov 22, 2019 7:54 AM UTC

Hi @Community member​,

TouchGFX can run on anything. Currently, CubeMX restricts user from selecting TouchGFX for anything that isn't an F4 and F7. That will change this december.

In the case of the WB there's no example from the designer or from CubeMX. I'm unsure if there's something in the Firmware pack for WB, but i doubt it.

Support through designer and CubeMX is coming. Until then, everything is possible, manually, but that could be a complex job for now.

/Martin

Remi QUINTIN
ST Technical Moderator
Nov 22, 2019 1:58 PM UTC

There is nothing preventing the use of TouchGFX on the STM32WB but the limitations could come from the richness of the graphics and the resulting number of graphical objects to manage.

Since STM32WB was not designed to offer rich graphic capabilities but support a wide range of wireless protocols, there is no example showing any graphical usage.