Skip to main content
HRidd.2
Associate
Mar 23, 2023 2:55 PM UTC
Question

Where is the platform implementation for HAL::initialize()?

I've been drilling down into some code used to initialize the touch controller in STM32TouchController::init(), but am having a lot of trouble finding where in ST's api actually calls this init() function. I can see that the initialize() method on the static instance of TouchGFXHAL is called, which calls the parent class TouchGFXGeneratedHAL::initialize(), which eventually calls the top level parent class touchgfx::HAL::initialize(). In HAL.hpp I can see that the touchcontroller reference touchCtrl is stored by reference in the member variable touchController:

/**
 * Initializes a new instance of the HAL class.
 *
 * @param [in] dmaInterface Reference to the DMA interface.
 * @param [in] display Reference to the LCD.
 * @param [in] touchCtrl Reference to the touch controller.
 * @param width The width of the LCD display, in pixels.
 * @param height The height of the LCD display, in pixels.
 */
 HAL(DMA_Interface& dmaInterface, LCD& display, TouchController& touchCtrl, uint16_t width, uint16_t height)
 : dma(dmaInterface),
 lcdRef(display),
 touchController(touchCtrl),
 mcuInstrumentation(0),
 buttonController(0),
 frameBufferAllocator(0),
 gestures(),
 nativeDisplayOrientation(ORIENTATION_LANDSCAPE),
 taskDelayFunc(0),
 frameBuffer0(0),
 frameBuffer1(0),
 frameBuffer2(0),
 refreshStrategy(REFRESH_STRATEGY_DEFAULT),
 fingerSize(1),
 lockDMAToPorch(false),
 frameBufferUpdatedThisFrame(false),
 auxiliaryLCD(0),
 partialFrameBufferRect(),
 listener(0),
 lastX(0),
 lastY(0),
 touchSampleRate(1),
 mcuLoadPct(0),
 vSyncCnt(0),
 vSyncForFrame(1),
 vSyncCompensationEnabled(false),
 clientDirty(false),
 swapRequested(false),
 lastTouched(false),
 updateMCULoad(0),
 cc_begin(0),
 requestedOrientation(ORIENTATION_LANDSCAPE),
 displayOrientationChangeRequested(false),
 useAuxiliaryLCD(false),
 useDMAAcceleration(true),
 lastRenderMethod(HARDWARE)
 {
 instance = this;
 FRAME_BUFFER_WIDTH = DISPLAY_WIDTH = width;
 FRAME_BUFFER_HEIGHT = DISPLAY_HEIGHT = height;
 DISPLAY_ROTATION = rotate0;
 nativeDisplayOrientation = ((width >= height) ? ORIENTATION_LANDSCAPE : ORIENTATION_PORTRAIT);
 }

However, I can't for the life of me find the actual implementation of the parent class's initalize() function:

 /**
 * This function initializes the HAL, DMA, TouchController, and interrupts.
 *
 * @see configureInterrupts
 */
 virtual void initialize();

From trial and error this is definitely the function that ends up caling touchController.init(), I just can't find where it does this. Any help is greatly appreciated...

This topic has been closed for replies.