Skip to main content
ANauz.1
Senior
May 11, 2021
Question

Where are downloaded the template used by TouchGFX Designer?

Hello,

I'm working on an offline PC with no possibility to connect to the internet.

I would like to try TouchGFX Template.

I have another PC with internet connection where the templates are available. I would like to copy the directory containing the template from my internet PC to my offline PC, but I could not figured out where the template are download.

Any one know where to look?

Thank you

Antoine

This topic has been closed for replies.

2 replies

Romain DIELEMAN
ST Employee
May 12, 2021

Hi,

I will have to investigate a bit more but I don't think we have a link to a zip (that I can share) with all application templates, but only links to a single zip. I think you have to do them one by one :downcast_face_with_sweat: (or a script).

Here is the typical link to a tpa for an application template: http://sw-center.st.com/touchgfx/pacman/4.16.0/<NAME OF THE BOARD>/<NAME OF THE APPLICATION TEMPLATE VERSION>

So for the STM32F412G-DISCO it should be this: http://sw-center.st.com/touchgfx/pacman/4.16.0/STM32F412G-DISCO/STM32F412G-DISCO-3.0.3.zip

Once you download the zip files/tpa you can add them to TouchGFX Designer following this article.

  

/Romain

ANauz.1
ANauz.1Author
Senior
May 18, 2021

Thank you.

I there a way to explore the directory? Clicking on http://sw-center.st.com/touchgfx/pacman/4.16.0/ propose me to download a zip.

Is there a similar address where I can download the UI Template?

I manage to get template for one board copying the directory "user"/AppData/Roaming/TouchGFX-4.16.1/Download from my internet PC to my offline PC

Antoine