Skip to main content
ABricout
Associate III
January 7, 2021
Solved

When will cube MX touchGFX compatible with stm32h747xi?

  • January 7, 2021
  • 3 replies
  • 1150 views

Hello,

I am trying to create a project on cubeMX with touchGFX using the eval board stm32h747i-disco. I can program my graphic application from the touchGFX software but when I try to create a project from cubeMX, I cannot add touchGFX generator and in the release notes of the version 4.16 it says : "TouchGFX Generator was previously available for projects with dual Core MCUs H747* and H745* despite not being supported yet."

Do you have an idea of when it will be released, I saw on the forum that it was planned for Q4 2020?

Also can I get the project used by the touch GFX software to generate the binary that is programmed to the eval board when you create a graphic application

Thank you by advance

Best regards,

This topic has been closed for replies.
Best answer by Romain DIELEMAN

Hi,

TouchGFX 4.17 is now live along a new release of the TouchGFX Board Setup (new name for "Application template") for the STM32H747-disco board based on STM32CubeMX and with a STM32CubeIDE project.

/Romain

3 replies

Romain DIELEMAN
ST Employee
January 8, 2021

Hi,

With the release of CubeMX 6.1 dual core projects handle additional softwares. The TouchGFX team is currently working on having the TouchGFX Generator support dual cores. There are no estimated delivery date I am aware of unfortunately.

Which project are you refering to ? Are you talking about the out-of-the-box demo ? If yes, it is found in the repository folder of CubeMX : user/STM32Cube/Repository/STM32Cube_FW_H7_V1.8.0/Projects/STM32H747I-EVAL/Demonstrations/

Best regards,

Romain

Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
July 2, 2021

Hi,

TouchGFX 4.17 is now live along a new release of the TouchGFX Board Setup (new name for "Application template") for the STM32H747-disco board based on STM32CubeMX and with a STM32CubeIDE project.

/Romain

CN.1
Associate
July 28, 2021

When will the STM32H745I-DISCO board be supported? Or what do I need to change to make one of the other examples work on the H745?