Skip to main content
RHitt.2
Associate II
November 23, 2020
Solved

When will a working project setup for STM32H747-DISCO and TouchGFX be available with CUBE-IDE ?

Actual version 1.5.0 of CUBE-IDE is a fail with respect to the above mentioned configuration (STM32H747-DISCO and TouchGFX)

This topic has been closed for replies.
Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
July 2, 2021

Hi,

TouchGFX 4.17 is now live along a new release of the TouchGFX Board Setup (new name for "Application template") for the STM32H747-disco board based on STM32CubeMX and with a STM32CubeIDE project.

/Romain

3 replies

Alexandre RENOUX
Visitor II
November 27, 2020

Hello,

Creating an Application Template for both the H747-DISCO and EVAL boards is in our plans. However, it has not been scheduled yet. I would say that a working Application Template could be done for Q1 2021 but again I cannot guarantee anything.

Sorry for the inconvenience,

/Alexandre

Martin KJELDSEN
Principal III
November 30, 2020

Hi,

I've just disabled X-CUBE-TOUCHGFX for H747/745 - It was a mistake to allow users to configure TouchGFX for it yet. Since CubeMX just added support for dual cores we'll need some time to make adjustments. We're starting work on it start of next year.

/Martin

Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
July 2, 2021

Hi,

TouchGFX 4.17 is now live along a new release of the TouchGFX Board Setup (new name for "Application template") for the STM32H747-disco board based on STM32CubeMX and with a STM32CubeIDE project.

/Romain