Skip to main content
sryuj.1
Visitor II
December 18, 2020
Question

When using the STMF479, if the MIPI function is not used, can the corresponding pins be left unconnected?

..

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
December 18, 2020

Yes, just leave the corresponding DSIHOST pins unconnected.

However, please note the information in the data sheet (Section 2.18).:

If DSI functionality is not used at all, then:

  • VDDDSI pin must be connected to global VDD.
  • VCAPDSI pin must be connected externally to VDD12DSI but the external capacitor is no more needed.
  • VSSDSI pin must be grounded

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.