Skip to main content
sryuj.1
Visitor II
December 18, 2020
Question

When using the STMF479, if the DHIHOST function is not used, can the corresponding pins be left unconnected?

..

This topic has been closed for replies.

1 reply

ST Technical Moderator
December 18, 2020

Hello @sryuj.1​ ,

I advise you to refer to the STM32F479xx Datahseet relevent for your device for more clarification on DSI Host functionality.

This document will guide you to configure the pins, and you will find this detail:

"If DSI functionality is not used at all, then:

  • VDDDSI pin must be connected to global VDD. 
  • VCAPDSI pin must be connected externally to VDD12DSI but the external capacitor is no more needed.
  • VSSDSI pin must be grounded.

"

You have also this helpful guide AN4860 Application note DSI Host on STM32F469/479, STM32F7x8/x9 and STM32L4R9/S9 MCUs.

Hope this helps you, and please don’t hesitate to come back for more clarification or any question.

Please mark my answer as best by clicking on the "Select as Best" button if it fully solved your issue. This will help other users find this solution more quickly.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks