Hi @Ebun.1,
Using a different operating system requires two things, generally:
- Implement the hooks provided by the OSWrappers interface.
- Write code to start touchgfx in a task for your OS
The interface for OSWrappers is as follows:
#ifndef OSWRAPPERS_HPP
#define OSWRAPPERS_HPP
#include <touchgfx/hal/Types.hpp>
namespace touchgfx
{
class OSWrappers
{
public:
/**
* @fn static void OSWrappers::initialize();
*
* @brief Initialize frame buffer semaphore and queue/mutex for VSYNC signal.
*
* Initialize frame buffer semaphore and queue/mutex for VSYNC signal.
*/
static void initialize();
/**
* @fn static void OSWrappers::signalVSync();
*
* @brief Signal that a VSYNC has occurred.
*
* Signal that a VSYNC has occurred. Should make the vsync queue/mutex available.
*
* @note This function is called from an ISR, and should (depending on OS) trigger a
* scheduling.
*/
static void signalVSync();
/**
* @fn static void OSWrappers::waitForVSync();
*
* @brief This function blocks until a VSYNC occurs.
*
* This function blocks until a VSYNC occurs.
*
* @note This function must first clear the mutex/queue and then wait for the next one to
* occur.
*/
static void waitForVSync();
/**
* @fn static void OSWrappers::takeFrameBufferSemaphore();
*
* @brief Take the frame buffer semaphore.
*
* Take the frame buffer semaphore. Blocks until semaphore is available.
*/
static void takeFrameBufferSemaphore();
/**
* @fn static void OSWrappers::tryTakeFrameBufferSemaphore();
*
* @brief Attempt to obtain the frame buffer semaphore.
*
* Attempt to obtain the frame buffer semaphore. If semaphore is not available, do
* nothing.
*
* @note must return immediately! This function does not care who has the taken the semaphore,
* it only serves to make sure that the semaphore is taken by someone.
*/
static void tryTakeFrameBufferSemaphore();
/**
* @fn static void OSWrappers::giveFrameBufferSemaphore();
*
* @brief Release the frame buffer semaphore.
*
* Release the frame buffer semaphore.
*/
static void giveFrameBufferSemaphore();
/**
* @fn static void OSWrappers::giveFrameBufferSemaphoreFromISR();
*
* @brief Release the frame buffer semaphore in a way that is safe in interrupt context. Called
* from ISR.
*
* Release the frame buffer semaphore in a way that is safe in interrupt context.
* Called from ISR.
*/
static void giveFrameBufferSemaphoreFromISR();
/**
* @fn static void taskDelay(uint16_t ms);
*
* @brief A function that causes executing task to sleep for a number of milliseconds.
*
* A function that causes executing task to sleep for a number of milliseconds.
* This function is OPTIONAL. It is only used by the TouchGFX in the case of
* a specific frame refresh strategy (REFRESH_STRATEGY_OPTIM_SINGLE_BUFFER_TFT_CTRL).
* Due to backwards compatibility, in order for this function to be useable by the HAL
* the function must be explicitly registered:
* hal.registerTaskDelayFunction(&OSWrappers::taskDelay)
* @param ms The number of milliseconds to sleep
* @see HAL::setFrameRefreshStrategy(FrameRefreshStrategy s)
* @see HAL::registerTaskDelayFunction(void (*delayF)(uint16_t))
*/
static void taskDelay(uint16_t ms);
};
} // namespace touchgfx
#endif // OSWRAPPERS_HPP
You need to provide implementations for these functions that use OS primitives for your particular OS. I haven't tried creating one for MBED OS, but i'd be happy to help give some pointers.
/Martin