Skip to main content
Associate II
Oct 8, 2025 8:19 AM UTC
Question

When TouchGFX runs with ThreadX, it doesn't show multiple objects.

Hello Everyone!

I am running TouchGFX with ThreadX. When I add a new object, TouchGFX does not display anything.
The settings for TouchGFX are as follows:

1. ThreadX

LeonSu_0-1759910513858.png

2.TouchGFX

LeonSu_1-1759910549552.png

3.TouchGFX Designer

I just created a box for the background.

LeonSu_2-1759910800201.png

 

TouchGFX is working well.

 

TouchGFX doesn't display anything when I add an image to this screen, as shown below.

LeonSu_3-1759911449073.png

 

 

Could you please give me some suggestions? Thanks in advance.

This topic has been closed for replies.

1 reply

ST Technical Moderator
Oct 9, 2025 6:56 AM UTC

Hello @LeonSu.

Could you provide more details? E.g. on the following:

  1. Which (MCU are you using?
  2. Is it custom hardware or ST hardware?
  3. Are your images stored in internal or external flash?
  4. When you mention that TouchGFX is working well with the box in point 3 that means that the box is visible on the display when you flash the application, right?
  5. Have you tried to connect a debugger to see if/where the application stalls?

Best regards,
Johan