Skip to main content
Physwm2501
Associate
Jun 16, 2022 11:03 PM UTC
Question

When adding new widgets to a custom container i2c communication fails.

I've been having an odd issue where if I add any widgets into a custom container the i2c ADC devices stop responding. I've isolated it to the point where I can just add any default widget into the container and then run target in the designer to see the issue. Once I go back and delete that widget all functions resume working.

When I go to debug the issue in cubeide the issue is not reproducible. The code compiled within the IDE works as intended with or without the added widgets.

This topic has been closed for replies.

1 reply

Osman SOYKURT
ST Technical Moderator
Jun 24, 2022 9:25 AM UTC

Hello Physwm2501,

Could you give more information about your configuration please ?

  • Which board do you use ?
  • Which version of TouchGFX Designer do you use ?
  • Which version of STM32CubeMX do you use ?

Are you using a TouchGFX Board Setup or did you start your project from scratch?

/Osman

ST Software Developer | TouchGFX