Skip to main content
HAven.1
Associate
February 4, 2022
Question

What's the maximum screen resolution supported by TouchGFX. In the TouchGFX_brochure.pdf a limit of 1024 x 768 for STM32H7. Is this limit for STM32H7 or TouchGFX? Can 1280 x 720 @ 30fps be supported used as well?

..

This topic has been closed for replies.

3 replies

MM..1
Super User
February 4, 2022

TouchGFX is software to memory layer code, dont have limit.

With partial framebuffer mode you can control for example 4096x4096 ...

Hardware layer code isnt part of TouchGFX.

Romain DIELEMAN
ST Employee
February 7, 2022

Hi,

​

Yes like MM said this is a hardware limitation. I havn't tried such big displays with the partial framebuffer though so I don't know what the performances would look like :grinning_face_with_sweat: I can maybe redirect you to Riverdi (an ST partner) which has embedded displays with STM32H7s with up to 1280*800 display resolution. But be aware that there might be limitations to what you can do: for example the color depth, "huge" image rotation, swipe transitions...

/Romain

HAven.1
HAven.1Author
Associate
February 8, 2022

Thanks for the replies