Skip to main content
Hiram Hyman
Associate III
Aug 1, 2022 8:36 AM UTC
Question

What's the fix and what could cause such: fatal error: gui/screen1_screen/Screen1View.hpp: No such file or directory. I deleted nothing. SETUP: CubeIDE 1.7.0 TouchGFX 4.18.1 Development kit: STM32H747-Disco

..

This topic has been closed for replies.

3 replies

Hiram Hyman
Associate III
Aug 1, 2022 9:00 AM UTC

In addition to the above question: I noticed that the screen Screen1View is deleted from the drive somehow but, the Screen1Presenter is present. It's not in the recycle bin. I'm still working to fix it without developing a new 5 page UI.

Hiram Hyman
Associate III
Aug 2, 2022 3:21 AM UTC

To All,

I could not resolve my issue. However, thanks to the container property in Touchgfx and saving previously written code in advance, I managed to recreate the screens with code without any problems.

What I'm going to do from this point on is save a copy of the entire project. Let's see if it helps.

Thanks,

Hiram

Yoann KLEIN
ST Employee
Aug 8, 2022 9:41 AM UTC

Hello @Hiram Hyman​ ,

Nice to hear that you found a solution to your problem.

Let us know if you have other issues with your project.

/Yoann

Yoann KLEINST Software Developer | TouchGFX