Skip to main content
MSale.1
Senior
May 14, 2020
Question

What is the Max DCMI Pixel Clock on the STM32H743 at 480 MHz? Is it 96MHz or fixed to 80 MHz?

As far as i understood the DCMI on AHB2 bus which has speed of (CPU/2 ) so at 480 MHz it will be 240MHz and the DCMI pixel clock must respect the minimum ratio of 2.5 so at this clock i will get 96 MHz or it for some other reason its fixed at 80 MHz only

This topic has been closed for replies.