Skip to main content
LDuin.1
Associate
Sep 16, 2022 12:06 PM UTC
Question

What is the display (or it's timings) on the STM32H750B-DK?

..

This topic has been closed for replies.

4 replies

ST Technical Moderator
Sep 16, 2022 1:16 PM UTC

Hello @LDuin.1​ and welcome to the Community :)

Please have a look at this AN5020 Application note Digital camera interface (DCMI) for STM32 MCUs

I hope this resource is helpful for you.

Imen 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
LDuin.1
LDuin.1Author
Associate
Sep 16, 2022 1:37 PM UTC

Hello and thank you @Imen DAHMEN​.

Unfortunately this is not quite what I am looking for.

The STM32H750B-DK has an LCD display connected to the LTDC via the LCD interface according to chapter 6.15 of the user manual. I was wondering how to set up this display in STM32CubeMX (mostly I'm looking for the Synchronization for Width/Height parameters) so I can draw things on it from code.

Hopefully this is a bit clearer than the question I asked before :)

Lennard

Tesla DeLorean
Guru
Sep 16, 2022 2:10 PM UTC

STM32Cube_FW_H7_V1.9.1\Drivers\BSP\STM32H750B-DK\stm32h750b_discovery_lcd.c

STM32Cube_FW_H7_V1.9.1\Drivers\BSP\Components\rk043fn48h\rk043fn48h.h

RK043FN48H

Should be in the BOM, and the BSP files. I think the screen details/docs have been posted to the forum previously

/**
 * @brief RK043FN48H Size
 */
#define RK043FN48H_WIDTH ((uint16_t)480) /* LCD PIXEL WIDTH */
#define RK043FN48H_HEIGHT ((uint16_t)272) /* LCD PIXEL HEIGHT */
 
/**
 * @brief RK043FN48H Timing
 */
#define RK043FN48H_HSYNC ((uint16_t)41) /* Horizontal synchronization */
#define RK043FN48H_HBP ((uint16_t)13) /* Horizontal back porch */
#define RK043FN48H_HFP ((uint16_t)32) /* Horizontal front porch */
#define RK043FN48H_VSYNC ((uint16_t)10) /* Vertical synchronization */
#define RK043FN48H_VBP ((uint16_t)2) /* Vertical back porch */
#define RK043FN48H_VFP ((uint16_t)2) /* Vertical front porch */
 
/**
 * @brief RK043FN48H frequency divider
 */
#define RK043FN48H_FREQUENCY_DIVIDER 5 /* LCD Frequency divider */
...
 
/**
 * @brief Initializes the LTDC.
 * @param hltdc LTDC handle
 * @param Width LTDC width
 * @param Height LTDC height
 * @retval HAL status
 */
__weak HAL_StatusTypeDef MX_LTDC_Init(LTDC_HandleTypeDef *hltdc, uint32_t Width, uint32_t Height)
{
 hltdc->Instance = LTDC;
 hltdc->Init.HSPolarity = LTDC_HSPOLARITY_AL;
 hltdc->Init.VSPolarity = LTDC_VSPOLARITY_AL;
 hltdc->Init.DEPolarity = LTDC_DEPOLARITY_AL;
 hltdc->Init.PCPolarity = LTDC_PCPOLARITY_IPC;
 
 hltdc->Init.HorizontalSync = RK043FN48H_HSYNC - 1U;
 hltdc->Init.AccumulatedHBP = (RK043FN48H_HSYNC + (RK043FN48H_HBP - 11U) - 1U);
 hltdc->Init.AccumulatedActiveW = RK043FN48H_HSYNC + Width + RK043FN48H_HBP - 1U;
 hltdc->Init.TotalWidth = RK043FN48H_HSYNC + Width + (RK043FN48H_HBP - 11U) + RK043FN48H_HFP - 1U;
 hltdc->Init.VerticalSync = RK043FN48H_VSYNC - 1U;
 hltdc->Init.AccumulatedVBP = RK043FN48H_VSYNC + RK043FN48H_VBP - 1U;
 hltdc->Init.AccumulatedActiveH = RK043FN48H_VSYNC + Height + RK043FN48H_VBP - 1U;
 hltdc->Init.TotalHeigh = RK043FN48H_VSYNC + Height + RK043FN48H_VBP + RK043FN48H_VFP - 1U;
 
 hltdc->Init.Backcolor.Blue = 0xFF;
 hltdc->Init.Backcolor.Green = 0xFF;
 hltdc->Init.Backcolor.Red = 0xFF;
 
 return HAL_LTDC_Init(hltdc);
}

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..