Skip to main content
MŁask.1
Associate II
May 11, 2022 7:34 AM UTC
Question

What is setup for minimal current for LCD on STM32L073

I have LCD connected to Nucleo with STM32L073. I have configured the clocks and low power mode so with EVERYTHING turned off I get 1uA of current.

Now using cube ide I have added configuration for LCD:

 hlcd.Instance = LCD;
 hlcd.Init.Prescaler = LCD_PRESCALER_1;
 hlcd.Init.Divider = LCD_DIVIDER_31;
 hlcd.Init.Duty = LCD_DUTY_1_4;
 hlcd.Init.Bias = LCD_BIAS_1_3;
 hlcd.Init.VoltageSource = LCD_VOLTAGESOURCE_INTERNAL;
 hlcd.Init.Contrast = LCD_CONTRASTLEVEL_5;
 hlcd.Init.DeadTime = LCD_DEADTIME_0;
 hlcd.Init.PulseOnDuration = LCD_PULSEONDURATION_4;
 hlcd.Init.HighDrive = LCD_HIGHDRIVE_0;
 hlcd.Init.BlinkMode = LCD_BLINKMODE_OFF;
 hlcd.Init.BlinkFrequency = LCD_BLINKFREQUENCY_DIV8;
 hlcd.Init.MuxSegment = LCD_MUXSEGMENT_DISABLE;

And after that I get 15 uA of current. Datasheet on page 86 says that I should have 2.6uA of additional current for LCD driver.

How to initialize LCD display to achive what is in documentation?

This topic has been closed for replies.

2 replies

Walid ZRELLI
Visitor II
May 17, 2022 11:17 AM UTC

Hello @Maciej �?aski​ ,

You can refer to the following example provided under the L0 Firmware Package:

  • Path: Projects\STM32L073Z-EVAL\Examples\LCD\LCD_Blink_Frequency

I hope this helps.

BeST Regards,

Walid

Mvill.17
Associate III
Jul 13, 2022 7:46 PM UTC

Before entering the STOP you've to deinit the LCD. In the function which deinit the low level skip the function that disable the LCD and reconfig the pins as analog.

I did this and achieved exacly 2,6uA

Bye