Skip to main content
ETale.1
Associate II
July 20, 2020
Solved

Warning: This IP has no parameter to be configured. in touch gfx configuration

I get the error shown in the image when I enable touch gfx software in cubeMx, in the same question(https://community.st.com/s/question/0D53W0000037kqg/warning-this-ip-has-no-parameter-to-be-configured) I saw a reply that said reinstalling cubemx will help fixing the problem but for my case it didn't work and I'm still facing the issue

This topic has been closed for replies.
Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
July 22, 2020

If you are using a STM32F746G-disco board, you can create a project directly from designer with the correct Application Template. When you will generate the code from Designer, a cubeMX project will be created with all the initial configurations for you with TouchGFX enabled. I see that you have extra configs (like USB) set in your project. They are not automatically set in this AT version since they are not necessary for graphics, so you will have to do those again in this new CubeMX project.

/Romain

3 replies

Romain DIELEMAN
ST Employee
July 21, 2020

Hi,

I have tried your ioc file you sent on the other topic you linked. I could not replicate the error the user had.

Just to be sure, are you using an STM32F746G-disco board ? If yes, how did you create your project (from CubeMX or Designer)?

/Romain

ETale.1
ETale.1Author
Associate II
July 21, 2020

Hi Romain,Thanks for your reply

I created the project using CubeMx and when I wanted to configure the TouchGfx i faced that error

Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
July 22, 2020

If you are using a STM32F746G-disco board, you can create a project directly from designer with the correct Application Template. When you will generate the code from Designer, a cubeMX project will be created with all the initial configurations for you with TouchGFX enabled. I see that you have extra configs (like USB) set in your project. They are not automatically set in this AT version since they are not necessary for graphics, so you will have to do those again in this new CubeMX project.

/Romain