Skip to main content
Uc.2361
Associate II
Dec 5, 2019 7:28 AM UTC
Question

Vertical scrolling Issue on LCD, source is Camera interfaced with DCMI interface.

I have an issue with the vertical scrolling on the LCD. The video is not being stable on the screen. LCD resolution is 480*272.

Camera Decoder used ADV7180.

Source is from Camera which is interfaced with DCMI interface.

I have attached the Video , Please point me where exactly I am going wrong.

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Dec 5, 2019 9:07 AM UTC

Can't watch the video from device I'm using but would guess a disparity in the line totals or synchronization.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Uc.2361
Uc.2361Author
Associate II
Dec 6, 2019 9:26 AM UTC

Thank you for the quick response but I have checked the DCMI configurations and even configurations of the decoder. But not finding any clue where its going wrong.

After adjusting crop settings, now its scrolling down slowly.

waclawek.jan
Super User
Dec 7, 2019 5:10 AM UTC

VSYNC not connected or pin misconfigured in GPIO?

Measure waveform directly on VSYNC input pin of mcu (touching physically the pin itself - I am aiming at bad solder joints); read out and check content of respective GPIO pin.

I don't use DCMI so don't know how exactly it detects the syncs, if it's not edge- but level-sensitive, then maybe also VSYNC polarity is incorrectly set.

JW