Skip to main content
tushar_tp
Associate III
Jan 28, 2020 5:06 PM UTC
Question

V3.0 Templates status

Hello @Martin KJELDSEN​ 

Is it possible to have a list of the available templates for V3.0 Pinned at top of this discussion forum. In that way we can tracked which one are remaining and which ones are done.

May be a list with priority would also help.

For eg.

  • STM32H7BI-DK v.3.0.0 (done)
  • STM32F746-DISCO v.3.0.0 (done)
  • STM32F769I-DISCO v.3.0.0 (done)
  • STM32H743I-EVAL v.3.0.0 (in progress)

Thanks,

Tushar

This topic has been closed for replies.

7 replies

LMese.1
Associate
Jan 28, 2020 8:45 PM UTC

Absolutely great idea, I highly agree with you. STM32F769I-DISCO v.3.0.0 still has some issues, so I'd like to know when it will be fixed as soon as possible.

Martin KJELDSEN
Principal III
Jan 29, 2020 9:33 AM UTC

Are you referring to the issue with CubeIDE projects that have a few extra, unknown files, referenced?

LMese.1
Associate
Jan 29, 2020 9:46 AM UTC

Hi Martin. No, I'm referring to the plug/unplug STM32F769I-DISCO messed up graphics issue (not referenced files is not a problem for me). I'm waiting for templates v.3.0 since the rest of my project is made with CubeMX 5.5 / CubeIDE and I've spent a couple of days trying to integrate it with the older templates with no success. Templates 3.0 are fantastic and perfectly fit into the project, but this small issue still there. Anyway, thank you so much for your time you dedicate to support us.

Martin KJELDSEN
Principal III
Jan 29, 2020 9:33 AM UTC

That's a good idea - I'll look into it.