Skip to main content
Associate
Jun 22, 2023 10:06 AM UTC
Solved

V22 of Designer crashes

In the new designer

 - just create an empty simulator project,

- error indicator : 

Combination of Simulator & Blank UI failed

and designer crashes.

Worked on previous versions.

    This topic has been closed for replies.
    wvlBest answer
    Associate
    Jun 27, 2023 1:54 PM UTC

    Problem: using virtual box with windows 10, touchgfx designer is not working.

    Solution : install visual studio  and reinstall designer,.. seems to work now.

     

     

     

    5 replies

    Yoann KLEIN
    ST Employee
    Jun 26, 2023 1:32 PM UTC

    Hello @wvl,

    I cannot reproduce this issue.

    Could you try to uninstall and reinstall TouchGFXDesigner 4.22.0 ?

     

    Please let me know how it is going.

    Yoann KLEINST Software Developer | TouchGFX
    wvlAuthor
    Associate
    Jun 27, 2023 10:40 AM UTC

    Hi,

    i'm running windows in a virtual box on ubuntu machine and then it doesn't work.  Running it on a 'native' windows pc it works.

    Previous version are running under virtual box. Any idea why this one not?

     

    wvlAuthor
    Associate
    Jun 27, 2023 12:11 PM UTC

    Some more info: Converting a existing project was failing with "load freetype library" issue.  Seems project uses some libraries of visual studio.

    So i installed visual studio on my windows, and conversion is working. In first step, the designer crashes, and then the designer hangs, log attached

    Yoann KLEIN
    ST Employee
    Jun 27, 2023 2:38 PM UTC

    Hello,

    Indeed, we use Visual Studio for building the simulator. So I guess that there was some mismatch or missing files in your VM that your application using TouchGFX Simulator was try to access, without success.

    For the TouchGFXDesigner crash part, it is not related to your VM, but it is a bug in this version of TouchGFXDesigner. The team is aware of it and is working on a patch.

    Glad that you find a solution to your issues though !

    Yoann KLEINST Software Developer | TouchGFX