Skip to main content
JPabl.1
Associate III
Nov 4, 2024 1:49 PM UTC
Solved

Using while to wait after a button is clicked crashes the ui

Hi there Touchgfx team!

I have this UI requirement to pop up a progress bar after the "read" button is clicked 

JPabl1_1-1730728041951.png

The progress bar will appear and go from 0 to 100 in 10 seconds. What I would like to do is that after the "read" button is clicked, I want to wait 10 seconds before continuing with the rest of the code. I tried a while but it crashes the UI. Here's my code: 

 

void calibrateView::read_calibration_step_flex_button_is_clicked()
{
 if (test_selected == QGA)
 {
 /* 1. send calibration read step to backend to get the value, This step can be triggered several times*/
 int calibration_rlu_atp1_value = presenter->notify_backend_read_calibration_step();

 // start_rlu_progress_bar_animation = true;
 customProgressBar.setVisible(true);
 customProgressBar.invalidate();
 start_rlu_progress_bar_animation = true;

this is where I want to wait the 10 seconds

 Unicode::UnicodeChar tempBuffer[20];
 Unicode::snprintf(tempBuffer, 20, "%d", calibration_rlu_atp1_value);
 update_text_buffer(rlu_atp_value_textBuffer, tempBuffer, RLU_ATP_VALUE_TEXT_SIZE, rlu_atp_value_text);

 // Swap the X and Y positions of the two buttons
 update_button_position(read_calibration_step_flex_button, upper_button_x, upper_button_y);
 update_button_position(proceed_flex_button, bottom_button_x, bottom_button_y);

 update_button_state(proceed_flex_button, true, true);
 update_button_state(read_calibration_step_flex_button, false, true);
 }
}

 

Thanks a lot in advance

This topic has been closed for replies.
GaetanGodart
GaetanGodartBest answer
ST Employee
Nov 5, 2024 1:36 PM UTC

Hello @JPabl.1 ,

 

You should not use wait() when you want to delay or use timing in TouchGFX.
Instead, use the function HandleTickEvent() that get's called every tick (60 ticks per second by default).

Please find attached an example of what you seems to want to achieve.
When clicking on the button, a progress bar appears and slowly goes from 0% to 100% over 10 seconds.

 

I hope this  helps! :smiling_face_with_smiling_eyes:
If this comment answers your question, I invite you to select it as "best answer".

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)

1 reply

GaetanGodart
GaetanGodartBest answer
ST Employee
Nov 5, 2024 1:36 PM UTC

Hello @JPabl.1 ,

 

You should not use wait() when you want to delay or use timing in TouchGFX.
Instead, use the function HandleTickEvent() that get's called every tick (60 ticks per second by default).

Please find attached an example of what you seems to want to achieve.
When clicking on the button, a progress bar appears and slowly goes from 0% to 100% over 10 seconds.

 

I hope this  helps! :smiling_face_with_smiling_eyes:
If this comment answers your question, I invite you to select it as "best answer".

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)