Skip to main content
FMarr.2
Associate III
November 24, 2020
Question

Using STM32CubeMX to setup LTDC: 1. If i resize the central area, when i visualize GPIO settings, it may happen that the vertical scroll bars are overloaded. It happens when the grid view width is bigger than the width of the hosting area

  1. Multiple selection of rows are intended or it is a side effect?
  2. Why if i set the same functionality on the pin view of one pin it disables the LTDC
  3. GPIO Settings, the pin configuration area should be vertically resizable

This topic has been closed for replies.