Skip to main content
Visitor II
Mar 4, 2026 9:21 AM UTC
Solved

Using qrcode with display BW 1bpp

I'm using an STM32G0 with a 240 x 160 monochrome 1bpp SPI display. Is it possible to use the QR code component from the TouchGFX library?

I'm using TouchGFX version 4.26.0.

Many thanks!

JohanAstrupBest answer
ST Technical Moderator
Mar 16, 2026 2:01 PM UTC

Hello @EmanueleC.

1bpp support is not implemented in the QR code widget currently bundled with TouchGFX. However, the widgets are open source, so you can add it yourself. You can find QRCode.cpp here: Middlewares\ST\touchgfx\framework\source\touchgfx\widgets

I recommend copying this file to gui\src\common and modifying the copy. The project will automatically use your version instead of the default one.

You’ll need to implement a draw function for 1bpp and then extend the switch statement in the draw function to call this 1bpp-specific function when the bit depth is 1:

void QRCode::draw(const Rect& invalidatedArea) const
{
 ...

 // Select correct drawing function for framebuffer format and alpha
 switch (bpp)
 {
 case 1:
 // Your 1bpp implementation goes here
 break;
 case 16:
 // RGB565
 drawfunc = (alpha < 255) ? &QRCode::drawBitRGB565Blend : &QRCode::drawBitRGB565;
 break;
 case 24:
 // RGB888
 drawfunc = (alpha < 255) ? &QRCode::drawBitRGB888Blend : &QRCode::drawBitRGB888;
 break;
 case 32:
 // ARGB8888
 drawfunc = (alpha < 255) ? &QRCode::drawBitARGB8888Blend : &QRCode::drawBitARGB8888;
 break;
 default:
 return;
 }

 ...
}

Best regards,
Johan

1 reply

JohanAstrupBest answer
ST Technical Moderator
Mar 16, 2026 2:01 PM UTC

Hello @EmanueleC.

1bpp support is not implemented in the QR code widget currently bundled with TouchGFX. However, the widgets are open source, so you can add it yourself. You can find QRCode.cpp here: Middlewares\ST\touchgfx\framework\source\touchgfx\widgets

I recommend copying this file to gui\src\common and modifying the copy. The project will automatically use your version instead of the default one.

You’ll need to implement a draw function for 1bpp and then extend the switch statement in the draw function to call this 1bpp-specific function when the bit depth is 1:

void QRCode::draw(const Rect& invalidatedArea) const
{
 ...

 // Select correct drawing function for framebuffer format and alpha
 switch (bpp)
 {
 case 1:
 // Your 1bpp implementation goes here
 break;
 case 16:
 // RGB565
 drawfunc = (alpha < 255) ? &QRCode::drawBitRGB565Blend : &QRCode::drawBitRGB565;
 break;
 case 24:
 // RGB888
 drawfunc = (alpha < 255) ? &QRCode::drawBitRGB888Blend : &QRCode::drawBitRGB888;
 break;
 case 32:
 // ARGB8888
 drawfunc = (alpha < 255) ? &QRCode::drawBitARGB8888Blend : &QRCode::drawBitARGB8888;
 break;
 default:
 return;
 }

 ...
}

Best regards,
Johan