Skip to main content
ELee.9
Associate II
Jan 16, 2023 2:31 AM UTC
Solved

Using dsi only one data lane with two data lane Touchscreen

Hi, I'm trying to use only one dsi data lane with OTM8009A which has two data lanes.

My MCU is STM32F769I-Eval and manuals said that this MCU has two dsi data lanes.

However, I want to use only one data lane because my custom board has only one dsi data lane.

I tried to change settings with Examples within F7Cube.

In LCD_DSI_Videomode_SingleBuffer, DSI Settings value is in there, so I change NumberOfLanes value two to one, but LCD Display doesn't work.

Is there any way to use only one data lane?

Thanks.

This topic has been closed for replies.
MM..1
MM..1Best answer
Super User
Jan 16, 2023 5:57 AM UTC

If display dont have this choice NO. Otherwise send init commands to display for setup one lane mode.

4 replies

MM..1
MM..1Best answer
Super User
Jan 16, 2023 5:57 AM UTC

If display dont have this choice NO. Otherwise send init commands to display for setup one lane mode.

ELee.9
ELee.9Author
Associate II
Jan 16, 2023 6:23 AM UTC

That means, If I couldn't modify the number of data lanes in display(in this case, OTM8009A), display will not work?

OTM8009A has two data lanes, and If I change the number of data lanes in STM32 to one, I think It will work strangely, but screen is only black.

When I change the number of data lanes in STM32 to two, It works properly.

MM..1
Super User
Jan 16, 2023 6:25 AM UTC

Simply you need change on both sides of bus...