Skip to main content
hbour
Visitor II
June 8, 2020
Question

use img file in a file syste rather than image generated by an image converter

Hello,

I plan to try to use your Graphic library on a custom board with a STM32H7

but first reading doc and use of touchdesigner

I'am asking if it is possible to use img that are stored in a file system ( sd card or qspi)

rather than image converted buy img converter an embedded in application flash ?

kind regards

heve

This topic has been closed for replies.

1 reply

Romain DIELEMAN
ST Employee
June 9, 2020

Hi,

It is possible to use images stored in a sd card but you will need to use dynamic bitmaps and bitmap caching. TouchGFX cannot render directly from a non-memory mapped flash (like an SD-card) so to overcome this limitation the bitmap cache provides a mechanism for caching some or all of the bitmap data in RAM during power-up. Here are the link to the articles on this: bitmap caching and dynamic bitmaps

If you have images in JPEG format for example you will need to add a loader, you can read more about it in this documentation. On the bottom of the page there is a link to a git repository with an example on how to use LibJPEG to use JPEG files.