Skip to main content
SPano.1
Associate
October 12, 2020
Question

Update GUI Model without RTOS inter-task messaging

Hi,

I need to update the GUI Model of touchGFX from another task that read data from some peripherals. I've seen that's recommended to use inter-task messaging system, like messaging queue, but unfortunately my RTOS doesn't implement anything like that yet.

What can I use to connect the Model class and other RTOS tasks?

This topic has been closed for replies.

2 replies

Martin KJELDSEN
Principal III
October 13, 2020

Which OS are you using?

SPano.1
SPano.1Author
Associate
October 14, 2020

ERIKA3. I've contacted the developers and they said me that it doesn't implement it yet, so I write a singleton class that could resolve my issue and act as a data queue for the Model GUI. Is there any "best practice" to use in situation like that?