Skip to main content
MillerWeldsJack
Associate
Mar 25, 2026 2:55 PM UTC
Solved

Unused Parameters in CompressedUnmappedFontCache and CompressedFontCache

I get the build warning (which is treated as an error):
```
CompressedUnmappedFontCache.cpp:146:66: error: unused parameter 'glyphNode' [-Werror=unused-parameter]
[build]   146 | void CompressedUnmappedFontCache::unableToCache(const GlyphNode* glyphNode, int byteSize)
```
This is easily fixed with
void CompressedUnmappedFontCache::unableToCache(const GlyphNode* /*glyphNode*/, int /*byteSize*/)
{
 while(1);
}​
But, it's generated code, so I have to make this fix every time a regenerate. This warning happens in both `CompressedUnmappedFontCache` and `CompressedFontCache`.
JohanAstrupBest answer
ST Technical Moderator
Mar 26, 2026 2:04 PM UTC

Hello .

Thank you for reporting this issue. I will make sure a fix is included in TouchGFX 4.27.0.

In the meantime, to avoid having to manually modify the generated code, you can create a Ruby script and run it from the Post Generate Target Command, which you can find under Config -> Build.

Best regards,
Johan

1 reply

JohanAstrupBest answer
ST Technical Moderator
Mar 26, 2026 2:04 PM UTC

Hello .

Thank you for reporting this issue. I will make sure a fix is included in TouchGFX 4.27.0.

In the meantime, to avoid having to manually modify the generated code, you can create a Ruby script and run it from the Post Generate Target Command, which you can find under Config -> Build.

Best regards,
Johan