Skip to main content
Associate
Jul 21, 2024 5:51 PM UTC
Question

Unresponsive Buttons on STM32F7 Disco After Holding Click

Hello everyone,

I added two buttons (the button type is shown in the attached picture) to my UI, each controlling two relays with the STM32F7 Disco. When I maintain a click on one of the buttons, both buttons turn off and become unresponsive. I need to reset the board to make them functional again.

Can anyone explain why the UI behaves this way and suggest a solution?

Thanks,

BR,

Nourhene.

NB1_0-1721584212032.png

 

This topic has been closed for replies.

3 replies

ST Employee
Jul 26, 2024 9:04 AM UTC

Hello @NB1 ,

In your code, how do you handle the switching between the buttons? I think it would be way easier to just use the Toggle Button widget in the TouchGFX designer which already implements the behavior you are looking for.

Please give it a try and test if the same issue still exists

Best regards, 

Mohammad MORADIST Software Developer | TouchGFX
NB1Author
Associate
Jul 26, 2024 3:51 PM UTC

Hello @Mohammad MORADI ESFAHANIASL,

Thank you for your response. I believe we are discussing the same widget. I am also using the button you mentioned, but the code I generated is slightly different from the code provided in this link: Toggle Button.

My question is: Could this difference be the reason for the issues I'm experiencing with my buttons?

Here is my generated code:

#include <gui_generated/screen1_screen/Screen1ViewBase.hpp>
#include <touchgfx/Color.hpp>
#include <images/BitmapDatabase.hpp>

Screen1ViewBase::Screen1ViewBase()
{
 __background.setPosition(0, 0, 800, 480);
 __background.setColor(touchgfx::Color::getColorFromRGB(0, 0, 0));
 add(__background);

 toggleButton1.setXY(345, 215);
 toggleButton1.setBitmaps(touchgfx::Bitmap(BITMAP_ALTERNATE_THEME_IMAGES_WIDGETS_TOGGLEBUTTON_MEDIUM_ROUNDED_ON_NORMAL_ID), touchgfx::Bitmap(BITMAP_ALTERNATE_THEME_IMAGES_WIDGETS_TOGGLEBUTTON_MEDIUM_ROUNDED_OFF_LIGHT_ID));
 add(toggleButton1);
}

Screen1ViewBase::~Screen1ViewBase()
{

}

void Screen1ViewBase::setupScreen()
{

}

 

ST Employee
Jul 30, 2024 8:24 AM UTC

I can see that you have assigned to action to your button.
How do you control the communication between the toggle and your relays? 

Mohammad MORADIST Software Developer | TouchGFX