Skip to main content
TLaur.3
Associate II
Jan 4, 2023 9:23 AM UTC
Solved

Unable to flash TouchGFX App on Riverdi RVT70HSSNWC00-B

Hello,

I've bought the Riverdi RVT70HSSNWC00-B STM32H7 embedded display.

But i'm unable to flash my app to the board.

Here are the log from touchGFX :

 -------------------------------------------------------------------
 STM32CubeProgrammer v2.11.0 
 -------------------------------------------------------------------
 
 ST-LINK SN : 39FF6D064E56363921500143
 ST-LINK FW : V2J40S7
 Board : --
 Voltage : 3.28V
 SWD freq : 4000 KHz
 Connect mode: Normal
 Reset mode : Software reset
 Device ID : 0x450
 Revision ID : Rev V
 Error: Database: There's no active configuration for this device. All the 8 configurations are disabled!
 Error: Database: There's no active configuration for this device. All the 8 configurations are disabled!
 Device name : STM32H7xx
 Flash size : 63 KBytes (default)
 Device type : MCU
 Device CPU : Cortex-M7
 BL Version : --
 
 
 
 Warning: Write address is ignored for hex, Srec, s19 and elf files
 
 
 Memory Programming ...
 Opening and parsing file: intflash.hex
 File : intflash.hex
 Size : 243.99 KB 
 Address : 0x08000000 
 
 
 Erasing memory corresponding to segment 0:
 Error: Unable to get core ID
 Erasing external memory sector 0
 Error: failed to erase memory
 
 
 Error: failed to erase memory
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.11.0 
 -------------------------------------------------------------------
 
 ST-LINK SN : 39FF6D064E56363921500143
 ST-LINK FW : V2J40S7
 Board : --
 Voltage : 3.09V
 SWD freq : 4000 KHz
 Connect mode: Normal
 Reset mode : Software reset
 Device ID : 0x450
 Revision ID : Rev V
 Error: Database: There's no active configuration for this device. All the 8 configurations are disabled!
 Error: Database: There's no active configuration for this device. All the 8 configurations are disabled!
 Device name : STM32H7xx
 Flash size : 63 KBytes (default)
 Device type : MCU
 Device CPU : Cortex-M7
 BL Version : --
 
 
 
 Memory Programming ...
 Opening and parsing file: extflash.bin
 Error: The file extflash.bin is empty
 
 Hard reset is performed
 make[2]: Leaving directory 'c:/TouchGFXProjects/MyApplication'
 make[1]: Leaving directory 'C:/TouchGFXProjects/MyApplication/gcc'
 Done

And here are the log from STM32CubeProgrammer:

0693W00000Y7NGvQAN.pngI'm a very beginner workins with STM32 and don't finda lot about these.

Can someone help me please ?

This topic has been closed for replies.
TLaur.3
TLaur.3Best answer
Associate II
Jan 4, 2023 3:12 PM UTC

I've found the solution. I used the ST-LINK/V2 Isolated version between the boardand my PC but it needs the non-isolated version of it to works. I took one on a nucleo board and it works weel.

Thanks for your answers @MM..1​ !

5 replies

MM..1
Super User
Jan 4, 2023 10:49 AM UTC

Try change Connect mode to Under reset

TLaur.3
TLaur.3Author
Associate II
Jan 4, 2023 12:30 PM UTC

I'm facing the same issue. And now I've a new error above "Error: Database..." :

"Error : Unable to get core ID"

MM..1
Super User
Jan 4, 2023 1:23 PM UTC

Try latest 2.12 version prog or an older.