Skip to main content
KMew
Senior III
Aug 11, 2022 7:13 PM UTC
Solved

Tutorial 2: Call New Virtual Function Overwriting Code

I am new to TouchGFX and STM32 programming, so I apologize if any obvious details are missed.

I am attempting to run Tutorial 2 in the TouchGFX tutorial (Because I'm a new member, I cannot add the link, but it's the TouchGFX Version 4 19 tutorial guide, Tutorial 2)

I have successfully run up to "Step 4: Adding Code."

I completed up to the step where it asks you to create the "buttonDown" interaction on the TouchGFX Designer (I'm running on 4 19 1).

I generate the code without issue, then it asks me to open MainViewBase.hpp (I was trying several screens, so mine is called Screen4ViewBase.hpp).

When I add the recommended code to display the "buttonUpClicked" and "buttonDownClicked" text pop up, I hit the "Run Simulation" button on the TouchGFX Designer and the code that I wrote disappears, so the text obviously does not appear.

Am I doing something wrong?

This topic has been closed for replies.
MM..1
MM..1Best answer
Super User
Aug 12, 2022 2:20 PM UTC

No this files is modified by generator when you move or change object in designer.

You can place code here, but every generation remove it.

Normal place code into folder GUI

4 replies

MM..1
Super User
Aug 12, 2022 4:59 AM UTC

Base file is generated code, and every Simulate or Generate click overwrite all generated files.

All your user code need be placed into GUI files Screen4View.hpp or cpp and other.

KMew
KMewAuthor
Senior III
Aug 12, 2022 1:24 PM UTC

Hello, thank you for the reply!

Just to make sure I understand, these are the files that I should modify, correct?

If so, these are the ones I tried and they are being overwritten.

0693W00000QNaE4QAL.png

MM..1
MM..1Best answer
Super User
Aug 12, 2022 2:20 PM UTC

No this files is modified by generator when you move or change object in designer.

You can place code here, but every generation remove it.

Normal place code into folder GUI