Skip to main content
dchen.2
Associate
May 26, 2021
Question

TOUCHGFX4.16.1 run target failed

...  Compile

       make -f ../gcc/Makefile -j8

       Reading TouchGFX/application.config

       Linking TouchGFX/build/bin/target.elf

       Producing additional output formats...

         target.hex  - Combined internal+external hex

         intflash.elf - Internal flash, elf debug

         intflash.hex - Internal flash, hex

         extflash.bin - External flash, binary

       Done

   Flash

       make -f ../gcc/Makefile flash -j8

       Reading TouchGFX/application.config

       Linking TouchGFX/build/bin/target.elf

       Producing additional output formats...

         target.hex  - Combined internal+external hex

         intflash.elf - Internal flash, elf debug

         intflash.hex - Internal flash, hex

         extflash.bin - External flash, binary

       d:/touchgfx_test/MyApplication_13/gcc/include/flash_sections_int_ext.mk:2: recipe for target '_extflash_' failed

       make[1]: *** [_extflash_] Error 5

       make: *** [flash] Error 2

       ../gcc/Makefile:52: recipe for target 'flash' failed

       Failed

   Failed

ps:

STM32F746G_ DISCO board.

touchgfx set up at D:\TouchGFX\4.16.1.

stm32cubeprogrammer set up at D:\Program .Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer (the latest 2.7.0 version)

The firmware version of ST- LINK is v2J37M27.

  D:\touchgfx_test\MyApplication_13\gcc\include\cube_programmer.mk line 7&8

program_files_win32 = /c/Program Files (x86) --> program_files_win32 = /d/Program Files (x86)

program_files_win64 = /c/Program Files --> program_files_win64 = /d/Program Files

Using the stm32cubeprogrammer sofeware, open D:\touchgfx_test\MyApplication_13\TouchGFX\build\bin\target.hex, download, It is ok.

This topic has been closed for replies.

2 replies

Romain DIELEMAN
ST Employee
May 27, 2021

Hi,

Are you using a custom project or did you start from the application template for the STM32F746G_DK available in TouchGFX Designer ? I was not able to reproduce your issue, could you check the revision of your board ? Look for a white sticker with "MB1191 <revision> ". Could you maybe share your project if not confidential ?

/Romain

dchen.2
dchen.2Author
Associate
May 27, 2021

Hi,

    I am using the application template for the STM32F746G_DK from TouchGFX Designer.  The board mode is MB1191B. I can not  run target in Touchgfx.(In PC, "Run simulator" is ok. And "Run target" mode. Only programmer is bad. the other is ok.because the output file"target.hex" is ok.)  . About my project.see attachment.