Skip to main content
Senior
Nov 29, 2024 2:23 PM UTC
Solved

TouchGFX Wildcard Issues displaying floating point data?

Hi all.  I'm trying to display local floating point variable data via a button click in text area fields on my TouchGFX project screen.  

I seem to be having an issue.   It appears that the fields are being populated with the format specifier that preceeds the variable in my code.  Here is my button function:  

void main_screenView::s_type_bobbin_btn_click()
{
 // Test constant, floating-point variables for bobbin dimensions
 const float bobbin_length = 12.51;
 const float bobbin_width = 7.36;
 const float bobbin_height = 3.88;

 // Convert the float values to strings and store them in the buffers
 Unicode::snprintf(bobbin_length_data_areaBuffer, sizeof(bobbin_length_data_areaBuffer), "%.2f", bobbin_length);
 bobbin_length_data_area.invalidate();

 Unicode::snprintf(bobbin_width_data_areaBuffer, sizeof(bobbin_width_data_areaBuffer), "%.2f", bobbin_width);
 bobbin_width_data_area.invalidate();

 Unicode::snprintf(bobbin_height_data_areaBuffer, sizeof(bobbin_height_data_areaBuffer), "%.2f", bobbin_height);
 bobbin_height_data_area.invalidate();
}

Here is the result of the button click (using the asterisk as a fallback character): 

Screenshot bobbin data6.png

I have tried multiple ways to try to correct this behaviour without success.  If anyone can shine a light on my errors/issues, I would be exteremely appreciative.  Thanks

 

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 29, 2024 2:34 PM UTC

Hello,

Use snprintfFloat instead of snprintf

Refer to: https://support.touchgfx.com/docs/api/classes/classtouchgfx_1_1_unicode

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

3 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 29, 2024 2:34 PM UTC

Hello,

Use snprintfFloat instead of snprintf

Refer to: https://support.touchgfx.com/docs/api/classes/classtouchgfx_1_1_unicode

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Al-E-BagsAuthor
Senior
Nov 29, 2024 2:47 PM UTC

Yay! So simple.  Thanks for the super quick response! Fixed it.