Skip to main content
DOkaz.1
Associate II
Jul 27, 2022 1:03 AM UTC
Solved

TouchGfx widget internet connectivity

Hi,

I want to connect a display powered by TouchGFX to a PC via usb-c. Is it possible to allow internet connectivity for a GUI widget via the usb-c connection to the host PC?

Thanks!

This topic has been closed for replies.
Piranha
PiranhaBest answer
Principal III
Jul 29, 2022 10:25 PM UTC

7 replies

MM..1
Super User
Jul 27, 2022 4:15 PM UTC

TouchGFX dont have prepared widget , but your code can use internet your way.

DOkaz.1
DOkaz.1Author
Associate II
Jul 29, 2022 7:45 PM UTC

How would the widget connect to the internet? does the board require its own TCP/IP stack chip? or is there a way todo like REST API calls or some other way to communicate over the internet?

Just trying to figure out if there is some pre-existing infrastructure that I can use or if it would need to be coded from scratch. or require some external hardware

Thanks!

Piranha
PiranhaBest answer
Principal III
Jul 29, 2022 10:25 PM UTC
DOkaz.1
DOkaz.1Author
Associate II
Jul 29, 2022 11:58 PM UTC

that looks like what I'm looking for, i'll look more into it. Thanks!

MM..1
Super User
Jul 31, 2022 11:01 AM UTC

Why not board or STM with ethernet ? Is more simple as USB C

STM32 Nucleo Boards - STMicroelectronics

DOkaz.1
DOkaz.1Author
Associate II
Aug 10, 2022 3:30 AM UTC

The usecase I have will only have a usb-c port as its interface, so having a full ethernet port would be a lot easier but wouldn't fit in the overall design

MM..1
Super User
Aug 10, 2022 2:19 PM UTC

Then yes STM have in USB CDC ECM and NDIS... Examples on github