Skip to main content
VK Verma
Associate III
May 18, 2019 5:39 PM UTC
Question

Touchgfx visual studio compilation error "Severity Code Description Project File Line Suppression State Error LNK1104 cannot open file "

Hi !

I am using touchgfx Version 4.10.0 and visual studio community 2019 version 16.0.4 and getting

"Severity Code Description Project File Line Suppression State

Error LNK1104 cannot open file '..\..\touchgfx\\lib\win\msvs\libtouchgfx_v142_debug.lib' Application D:\Technical_Docs\Touchgfx\GettingStarted7Inch\simulator\msvs\LINK 1"

when i build touchgfx simulator target. Please help me to resolve this.

Regards,

VK Verma

This topic has been closed for replies.

9 replies

Martin KJELDSEN
Principal III
May 20, 2019 8:20 AM UTC

Hi, you're trying to link with a Visual Studio 2019 library (v142) which is not a part of any release of TouchGFX yet. 4.10.0 was released a while ago and MSVS v142 is relatively new. The latest supported version in that release is v141 (MSVS 2017).

Keep an eye out for a new TouchGFX release :)

/Martin

VK Verma
VK VermaAuthor
Associate III
May 20, 2019 4:42 PM UTC

Hi Martin,

Thanks for your valuable reply, and I tried my best to download community edition of MSVB-2017 but microsoft does not provide any download link for new installations of MSV-2017.

Can you advice some alternative for this please!

Thanks and Best Regards,

VK verma

EKear
Visitor II
May 21, 2019 11:33 AM UTC

Hi,

I have being struggling with the same issue today, but I have managed to get a download of MSVS 2017 Community edition from Microsoft using the following link https://visualstudio.microsoft.com/thank-you-downloading-visual-studio/?sku=Community&rel=15

The number on the end is the revision number (2019 is revision 16).

I hope this helps

Erik

VK Verma
VK VermaAuthor
Associate III
May 21, 2019 12:00 PM UTC

Hi @EKear​ 

With your kind support and after installing few plugins with change in SDK version. I am able to build touchgfx with MSVS2017 with zero build errors.

I think your post will help many more like us as all new user on touchfgx will definitely stuck there.

Thanks for your support!

Regards,

VK Verma:)

Uday Kiran
Associate
Sep 27, 2019 7:28 AM UTC

@Martin KJELDSEN​ 

Can you approximate date of v142.debug version availability. Will it me done in month or two ?