Skip to main content
RThom.5
Visitor II
May 12, 2021
Question

TouchGFX Using SPI with STM32H7

Hey There,

I am working on a project that will involve using a STM32H743VIT6. Its quite a complex board so almost all of the pins one the MCU have been occupied. Because of this I have to drive the 240x320 LCD-TFT with SPI ( Driver is ILI9341). I was hoping to use the ChromeART graphics accellerator to do this to relieve the load on the MCU. However I just came accross this https://support.touchgfx.com/docs/development/hardware-selection/hardware-components/hardware-selection-mcu which only lists Parallel, LCD-TFT and MIPI DSI as the ChromART peripherals for the STM32H7 series.

Would there be any way of redirecting the output of one of these peripherals so that it would work with an SPI channel?

Thanks

Ricky

This topic has been closed for replies.