Skip to main content
Associate III
Mar 21, 2026 7:39 AM UTC
Solved

TouchGFX UI works in simulator but not displaying on STM32H7B3I-EVAL TFT (only backlight ON)

Hello,

The board revision I am using is MB1370-lcd-b02 a254300030.

I am working with the STM32H7B3I-EVAL board and using TouchGFX (TouchGFX Designer).

I have created a simple screen in TouchGFX, and:

  • The simulation runs correctly on PC
  • The project builds successfully in STM32CubeIDE
  • The code flashes successfully to the board

However, on hardware:

  • The TFT backlight turns ON
  • But no UI is displayed (screen is blank)
JohanAstrupBest answer
ST Technical Moderator
Mar 23, 2026 7:38 AM UTC

Hello @vijayajangam.

Which board revision do you have? You can find it on a sticker on the underside of the board.

I have just tested with the board I have here, and it works fine. The board revision I am using is MB1331-H7B3LIQ-D03.

Best regards,
Johan

17 replies

JohanAstrupBest answer
ST Technical Moderator
Mar 23, 2026 7:38 AM UTC

Hello @vijayajangam.

Which board revision do you have? You can find it on a sticker on the underside of the board.

I have just tested with the board I have here, and it works fine. The board revision I am using is MB1331-H7B3LIQ-D03.

Best regards,
Johan

Visitor II
Mar 29, 2026 10:39 PM UTC

Hello @JohanAstrup  I’m experiencing the same issue on my side.

In my case, I’m using the STM32H7B3I-EVAL D04 board revision.

The project compiles and flashes correctly, but nothing is displayed on the screen (black screen / backlight only). The TouchGFX simulator works fine.

For reference, here are my versions:

  • TouchGFX Designer: 4.26.1

  • Demo version: v3.0.17

  • STM32 MCU Package: v1.13.0

  • STM32CubeMx Version: v6.17.0

I suspect this might be related to external memory initialization or loader configuration, but I haven’t found a clear solution yet.

Has anyone managed to get this working with this combination of versions and board revision?

Any guidance would be appreciated.

ST Technical Moderator
Apr 8, 2026 9:29 AM UTC

Was there an application already running on the board when you received it?

How are you powering the board? With this specific EVAL board, I sometimes experience issues if I do not use an external power supply, as the board requires quite a lot of power. Please remember to set the jumper correctly according to your setup on the pins between the DC jack and the RS232 connector.

Could you also try to run one of the demos from the firmware pack? For example the one placed here:
C:\Users\YOUR_USER_NAME\STM32Cube\Repository\STM32Cube_FW_H7_V1.13.0\Projects\STM32H7B3I-EVAL\Examples\LTDC\LTDC_ColorKeying.

Best regards,
Johan

ST Technical Moderator
Apr 13, 2026 2:03 PM UTC

Hello again.

I have investigated this a bit further. Since I do not have the correct hardware yet, I am unfortunately unable to verify the issue.

However, as far as I can see, the touch driver has been changed from FT5336 to GT911 on D04. Since the TBS available in TouchGFX Designer uses BSP code, there is a good chance that this could cause a hardfault. I do not know whether you have tried debugging the application to see what happens .. ?
You can quickly verify whether this resolves the issue by commenting out the contents of TouchGFX/target/STM32TouchController.cpp.

If this is indeed the issue, then there are two ways to fix this:

1. We previously had the exact same case with the STM32H735G-DK. This was fixed in version 3.0.22 of the TBS. You could look at TouchGFX/target/STM32TouchController.cpp in that project and try to replicate the behavior.

2. Update to the latest version of the BSP, which you can find in the firmware package.

Unfortunately, I cannot guarantee that the touch driver is the only issue until I get the new revision. Once we receive the new revision, we will update the relevant projects available in TouchGFX Designer.

Please let me know once you have had time to test it. Thank you!

Best regards,
Johan

Associate III
Apr 14, 2026 5:50 AM UTC

Hello  JohanAstrup

my touch gfx project zip attatched here please find it and give me proper solution.

The board revision I am using is MB1370-lcd-b02 a254300030.

 

Thanks

Vijaya

Vijaya
mƎALLEm
ST Technical Moderator
Apr 20, 2026 10:35 AM UTC

Hello,

It could be the something related to the external flash. So the assets are not uploaded to the external flash.

Check what CubeIDE is saying when uploading your application to the board.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate III
Apr 21, 2026 9:49 AM UTC

Hello,

Touch GFX is suport dirrectly flash code into controller or need STM32cube IDE for generate output file dirreclty from TOuch GFX uplaod the code into controller.

 

Thanks.

Vijaya.

Vijaya
ST Technical Moderator
Apr 21, 2026 11:13 AM UTC

Hello @vijayajangam.

There have recently been similar reports of this issue. It appears that the touch driver was changed in the latest board revision, introducing breaking changes to the software.

I have attached a project in which I updated the latest TBS to the newest version of the BSP code. Please validate and confirm whether this resolves your issue. If it does, I will upload a new version of the TBS with this fix.

Best regards,
Johan

Associate III
Apr 22, 2026 8:06 AM UTC

Hello ,

please upload a new version of the TBS with this fix. 

Thank You

Vijaya.

Vijaya
ST Technical Moderator
Apr 21, 2026 11:17 AM UTC

Hello again.

This is a duplicate of this this ticket. Please refer to the solution proposed there.

Best regards,
Johan

ST Technical Moderator
Apr 22, 2026 8:10 AM UTC

I need you to confirm that it works before I can upload it.
Could you please test the previously attached project and let me know whether it fixes the issue?

Best regards,
Johan

Associate III
May 12, 2026 8:04 AM UTC

no my issue not yet solve 

Vijaya
ST Technical Moderator
May 15, 2026 8:31 AM UTC

New versions of both the STM32H7B3I-EVAL TBS and BSD, which support newer board revisions, have now been uploaded to TouchGFX Designer.

The new TBS version is 3.0.21, and the new BSD version is 3.0.18. Please check and confirm whether these versions work on your board.

Best regards,
Johan

Associate III
Oct 28, 2026 11:45 AM UTC

Hello

My WIFI module still not working give me solution with emo code 

 

Thank You,

Vijaya Jangam.

Vijaya