Skip to main content
Ameya M
Associate III
Jul 15, 2019 2:15 PM UTC
Question

TouchGFX support for 32F723EDISCOVERY ST developer kit for UI development

Hello,

We want to use 32F723EDISCOVERY having Frida FRD154BP2902-CTP LCD display.

On the TouchGFX designer it's application template is not available and also it's not listed in supported ST kits on the website.

https://www.touchgfx.com/product/supported-stm32-kits/

Can we create custom template for 32F723EDISCOVERY in TouchGFX for GUI development and how easy would it be?

Also what kind of support is available if custom template can be created.

If not, are there any other IDEs/Development tools for 32F723EDISCOVERY GUI Development from ST/elsewhere.

Thanks,

Ameya

This topic has been closed for replies.

7 replies

Anders Nedergaard PETERSEN
Senior II
Jul 16, 2019 9:36 AM UTC

Hi @Ameya M​ ,

You can create your own Application Template which can be loaded by the TouchGFX Designer, please use this link: https://touchgfx.zendesk.com/hc/en-us/articles/115002741432-Create-custom-Application-Template

Even though the board is not listed on the supported stm32 kits, a port for the board is still possible ;)

Please see, https://touchgfx.zendesk.com/hc/en-us/articles/204993902-Porting-to-STM32F4-F7-boards for porting for F7.

The mcu you are targeting does not have graphical hardware acceleration and therefore all rendering will be done in software by the MCU!

I suggest you take a look in the STM32F7Cube package and find the example application configuring the LCD, this is located in Projects\STM32F723E-Discovery\Applications\STemWin.

If you wish to use TouchGFX instead of STemWin you can use the porting guide mentioned above to add the TouchGFX framework to the application.

/Anders

Ameya M
Ameya MAuthor
Associate III
Jul 16, 2019 10:45 AM UTC

Hello @Anders Nedergaard PETERSEN​ ,

Thank You for the reply.

The application is very space critical, hence we wanted this type of controller which does not need external RAM, etc. for Graphics.

We want standalone controller due to which overall form factor will be reduced.

But as you have mentioned in your reply, the target MCU does not have graphical hardware acceleration, so the graphics quality may get compromised.

But we want good graphics with minimal or no external hardware.

Please suggest a MCU covering following points:

1) Is supported by TouchGFX (and preferably in LQFP package, avoid BGA packages), ideally having configured Application template in TouchGFX

2) Does not need external hardware for graphics like RAM, even if needed the form factor remains small.

3) Graphics quality is not compromised.

Awaiting your reply.

Thanks,

Ameya

Anders Nedergaard PETERSEN
Senior II
Jul 16, 2019 11:51 AM UTC

Hi @Ameya M​ 

In order to guide you better, I have a couple of questions regarding the application requirements.

a) Is the desired resolution the same as the display on 32F723EDISCOVERY and at what color depth would you like the application to run at?

b) What about power consumption, is it a battery power device?

c) Is the graphical application demanding, i.e. a lot of simultaneous animations or more static e.i. a menu like application?

You only mention that you want to avoid external RAM, what about external flash? - Using only internal flash will set a limitation on the amount of graphical assets you are able to use for the application.

/Anders