Touchgfx + STM32F411+ SPIFLASH
- 1 reply
- 300 views
Hi guys,
I'm working on custom board with STM32F411 + spiflash for a project with Touchgfx (partial buffer).
At the moment I got spiflash and STM32F411 working via SP1 + DMA and that's fine.
I'm using IAR 9.70 for this project and I'm facing an issue with external flash loader when I do a debugging session.
When I start a debugging session, flash is programmed and the external loader programs the spiflash too.
But on the end of the programming the procedure fails with:
Sun Mar 29, 2026 21:45:19: Initial reset was performed
Sun Mar 29, 2026 21:45:19: Loaded debugee: C:\Program Files\IAR Systems\Embedded Workbench 9.2_3\arm/config/flashloader/ST/FlashSTM32F4xxxRAM128K.out
Sun Mar 29, 2026 21:45:19: Target reset
Sun Mar 29, 2026 21:45:26: Unloaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.2_3\arm/config/flashloader/ST/FlashSTM32F4xxx.mac
Sun Mar 29, 2026 21:45:26: Loaded macro file: D:\ARM\STM32F411\AlphaTui\CubeMx\AlphaTui\EWARM/icf/ExtSPIFLd.mac
Sun Mar 29, 2026 21:45:26: Loaded debugee: D:\ARM\STM32F411\AlphaTui\CubeMx\AlphaTui\EWARM/icf/ExtSPIFLd.out
Sun Mar 29, 2026 21:45:26: Target reset
Sun Mar 29, 2026 21:45:26: Unloaded macro file: D:\ARM\STM32F411\AlphaTui\CubeMx\AlphaTui\EWARM/icf/ExtSPIFLd.mac
Sun Mar 29, 2026 21:45:26: Downloaded D:\ARM\STM32F411\AlphaTui\CubeMx\AlphaTui\EWARM\AlphaTui\Exe\AlphaTui.out to flash memory.
Sun Mar 29, 2026 21:45:26: 227026 bytes downloaded into FLASH (28.38 Kbytes/sec)
Sun Mar 29, 2026 21:45:27: ELF/DWARF Error: Unknown
Sun Mar 29, 2026 21:45:27: Failed to load debugee: D:\ARM\STM32F411\AlphaTui\CubeMx\AlphaTui\EWARM\AlphaTui\Exe\AlphaTui.out
Sun Mar 29, 2026 21:45:27: Unloaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.2_3\arm/config/debugger/ST/STM32F4xx.dmac
Sun Mar 29, 2026 21:45:28: Loading the ST-LINK Driver driver
the debugging session is aborted and it seems that the debugger is unable to retrieve symbols.
If I put my spisflash data temporarly in flash and not in (0x90000000...0x907FFFFF) everything is ok and I can debug.
I'm sure that spiflash is programmed because I read it and the data are the desidered
Have you any idea what is going wrong?
Attached here I put my .board/flash/icf.
Thanks.