Skip to main content
papamidas
Associate II
August 14, 2021
Question

touchgfx + stm32cubeide: how to enable word- and code completion, content assist, parameter hints?

I am using TouchGfx 4.17 together with stm32cubeide 1.7.0.

Right at the moment I'm trying out all the TouchGfx tutorials.

I really like all the word- and code completion-, content assist. and parameter hints features of stm32cubeIDE, but it seems that none of these features work in a TouchGfx-Designer-generated project any more.

I can't find the right setting in stm32CubeIDE for enabling those features; it seems that they are already enabled but somehow refuse to work.

So, what settings in stm32cubeIDE should I change so that all the nice features that work perfectly with the HAL library also work with TouchGfx? 

This topic has been closed for replies.

2 replies

Alexandre RENOUX
Visitor II
August 19, 2021

Hello CRaus.1,

I added STM32CubeIDE as a topic because this is not directly linked to TouchGFX.

/Alexandre

Romain DIELEMAN
ST Employee
September 9, 2021

Hi,

Were you able to find how to enable those features ? Seems interesting.

/Romain