Skip to main content
Associate II
May 12, 2025 6:51 AM UTC
Solved

TouchGFX Specific board offline using

Hello,
I am working with STM32 TouchGFX on a Riverdi board. I would like to use the board-specific settings in offline mode. Are there any files available for specific boards? If so, is it possible to transfer those files via a flash drive and use TouchGFX with the specific board on a computer without internet access, by placing them in the appropriate directory?

This topic has been closed for replies.
GaetanGodart
GaetanGodartBest answer
ST Employee
May 12, 2025 9:10 AM UTC

Hello @hamzatamer ,

 

Yes you can import a board specific setup (or TBS for TouchGFX Board Setup) to a computer without internet access.

 

1)

If the setup you want to get is one of the TBS provided by TouchGFX in designer (a few nucleo boards + Riverdi displays have a TBS), you can just download the TBS on a computer with internet, then go to YourPath\AppData\Roaming\TouchGFX-YourVersion\Downloads\TBSname\TBSversion . There you will find the .tpa file of the project and that is the file you have to copy to the computer without internet (to the same appData/Roaming location).
So for example if I want to copy the STM32U5G9J-DK2 TBS, my path is C:\Users\Name\AppData\Roaming\TouchGFX-4.24.2\Downloads\STM32U5G9J-DK2\3.0.7 :

GaetanGodart_0-1747040798610.png

 

2)

If you are using a custom board and you want to import a working project for your specific board, then you need to create the .tpa file by following the TPA guide .

 

I hope this answers your question, if it does, please select this comment as "best answer".

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)

1 reply

GaetanGodart
GaetanGodartBest answer
ST Employee
May 12, 2025 9:10 AM UTC

Hello @hamzatamer ,

 

Yes you can import a board specific setup (or TBS for TouchGFX Board Setup) to a computer without internet access.

 

1)

If the setup you want to get is one of the TBS provided by TouchGFX in designer (a few nucleo boards + Riverdi displays have a TBS), you can just download the TBS on a computer with internet, then go to YourPath\AppData\Roaming\TouchGFX-YourVersion\Downloads\TBSname\TBSversion . There you will find the .tpa file of the project and that is the file you have to copy to the computer without internet (to the same appData/Roaming location).
So for example if I want to copy the STM32U5G9J-DK2 TBS, my path is C:\Users\Name\AppData\Roaming\TouchGFX-4.24.2\Downloads\STM32U5G9J-DK2\3.0.7 :

GaetanGodart_0-1747040798610.png

 

2)

If you are using a custom board and you want to import a working project for your specific board, then you need to create the .tpa file by following the TPA guide .

 

I hope this answers your question, if it does, please select this comment as "best answer".

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)