Skip to main content
Associate II
Jul 5, 2023 8:52 AM UTC
Solved

TouchGFX Roadmap

Hello,

I checked but I didn't find any information, is there a TouchGFX roadmap available somewhere ?

Regard,

NME

This topic has been closed for replies.
Osman SOYKURT
Osman SOYKURTBest answer
ST Technical Moderator
Jul 5, 2023 3:17 PM UTC

Hello @nme ,

You can check the changelog if you need to know what is new and what is deprecated between versions of TouchGFX. But concerning the roadmap, it's quite confidential I'm afraid. But you're more than welcomed to ask for features, we'll discuss about them internally and consider or not to develop them.

Hope that answers your question :)

ST Software Developer | TouchGFX

7 replies

Peter BENSCH
ST Technical Moderator
Jul 5, 2023 11:40 AM UTC

Welcome @nme, to the community!

What exactly do you mean by roadmap?
TouchGFX is constantly being developed further, e.g. vector graphics (SVG) have also been supported for a while. What function are you looking for specifically?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
nmeAuthor
Associate II
Jul 5, 2023 12:25 PM UTC

Hello Peter,

I use TouchGFX on a project release 4.16.1 and as we start a new project I start to use 4.22. There's a lot of new features especially L8 compression and stock.

But for example I wanna use a vertical swipe container which is not yet available. My concern was should I develop a container or will this be included in a next release, it's not an urgent need so if it will be in a next release I will not spend time on the feature.

Nicolas

Osman SOYKURT
Osman SOYKURTBest answer
ST Technical Moderator
Jul 5, 2023 3:17 PM UTC

Hello @nme ,

You can check the changelog if you need to know what is new and what is deprecated between versions of TouchGFX. But concerning the roadmap, it's quite confidential I'm afraid. But you're more than welcomed to ask for features, we'll discuss about them internally and consider or not to develop them.

Hope that answers your question :)

ST Software Developer | TouchGFX