Skip to main content
Hhuan.3
Associate III
Dec 2, 2022 8:36 AM UTC
Question

touchgfx question: Internal ram is not enough for touchgfx to use ;can it be changed to external ram?how to change?

..

This topic has been closed for replies.

8 replies

MM..1
Super User
Dec 2, 2022 1:40 PM UTC

MCU? Any code can use any designed ram, you need handle bus capacity. Use linker section for this.

Hhuan.3
Hhuan.3Author
Associate III
Jan 14, 2023 8:31 AM UTC

thanks for answer;i want to ask another question; Because the project is more complex, ui controls and containers are more, including text and dynamic text are many; HardFault_Handler freezes when adding text or ui images. The current test found that add a few dynamic text definition on crash, delete after normal; Also encountered after adding a picture crash, delete the picture after normal;i use touchgfx the verson is 4.20.0

Hhuan.3
Hhuan.3Author
Associate III
Jan 14, 2023 8:30 AM UTC

thanks for answer;i want to ask another question; Because the project is more complex, ui controls and containers are more, including text and dynamic text are many; HardFault_Handler freezes when adding text or ui images. The current test found that add a few dynamic text definition on crash, delete after normal; Also encountered after adding a picture crash, delete the picture after normal