Skip to main content
KMew
Senior III
Oct 30, 2023 1:49 PM UTC
Solved

TouchGFX: Only show part of an image

Hello,

I have a .png image that I'm using in the TouchGFX GUI (utilizing the STM32H725AGI6), which I have fully integrated with the display and working.

That image is going to dynamically change based on a specific value received from the code (0-100%). When it's 100%, the entire image is showing. When the value is 50%, the left half of the image is revealed and the right half will not be shown. When the value is 0%, the image is not showing. 

I was previously using a black box that was on a layer higher than the image and had it slowly cover it, but now I have a real background image and not a black box, so that is no longer feasible.

 

Is there a way to dynamically define how much of the image is drawn? Something similar to the image below.

KMew_0-1698673759728.png

KMew_1-1698673768435.pngKMew_2-1698673777363.png

 

 

This topic has been closed for replies.
MM..1
MM..1Best answer
Super User
Oct 30, 2023 6:47 PM UTC

1 reply

MM..1
MM..1Best answer
Super User
Oct 30, 2023 6:47 PM UTC