Skip to main content
Associate II
Dec 4, 2024 10:39 AM UTC
Solved

TOUCHGFX: is multi display possible ?

Hi,

For a project I am currently working on, we have a unique custom board model on which we can flash different targets of a a same program.
Depending on the target, we can work with one of two different displays, a 240x320 and a 160x80.
For now, we two project TouchGFX, one for each display.
I understood that it not possible for TouchGFX Designer to handle several physical displays. Is it still the case ?
If so, is there a way to get around it ?

S. Marie

This topic has been closed for replies.
GaetanGodart
GaetanGodartBest answer
ST Employee
Dec 10, 2024 2:02 PM UTC

Hello @SMarie ,

 

Indeed it is not possible to manage 2 screens with TouchGFX.

The walk around would be to make a GUI that is flexible by using scalable images, regular images with 2 assets (one for each size) and resize/load the right assets at the start of the GUI but this is definitely not what you should aim for in embedded projects.

The best answer is to simply make 2 projects, not so much because TouchGFX cannot handle it but because embedded projects are not meant to have this level of flexibility!

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)

2 replies

MM..1
Super User
Dec 7, 2024 8:23 AM UTC

Your title Q isnt clean , but primary TGFX manage only image in memory, nothing more. Your hw driver and config transfer it to display. Then swap is based on your detection code and management... = possible

And tip for designer create screens for display 1 and too screens for 2 , then on start determine what loaded...

GaetanGodart
GaetanGodartBest answer
ST Employee
Dec 10, 2024 2:02 PM UTC

Hello @SMarie ,

 

Indeed it is not possible to manage 2 screens with TouchGFX.

The walk around would be to make a GUI that is flexible by using scalable images, regular images with 2 assets (one for each size) and resize/load the right assets at the start of the GUI but this is definitely not what you should aim for in embedded projects.

The best answer is to simply make 2 projects, not so much because TouchGFX cannot handle it but because embedded projects are not meant to have this level of flexibility!

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)