Skip to main content
fog.1
Associate III
Oct 12, 2023 4:46 PM UTC
Solved

TouchGFX intelisense problems

 

intellisense is not working.  the components that I can't use the intellisense feature( button, Textarea, slider, scroolist and the like...) "Screen1ViewBase.it is observed that the text colors of the implementations in the "cpp" file are also different(not blue).

"Screen1View.when I try to use the corresponding component in the "cpp" file, the "ctrl+space" keys do not work, or rather, inteslisense cannot complete the code.

1.png

2.png

3.png

 

This topic has been closed for replies.
ST Employee
Oct 24, 2023 9:50 AM UTC

Hello @fog.1 ,

When your IDE is open and you add a new widget from the designer, you should regenerate code through the designer, so the files are updated to recognize the new widget you have added to your project. If the new widgets are still not recognized, try to close and reopen the project. But keep the code regeneration in mind.

I hope this helps you, and don't hesitate to ask more questions 

Mohammad MORADIST Software Developer | TouchGFX

3 replies

ST Employee
Oct 24, 2023 9:50 AM UTC

Hello @fog.1 ,

When your IDE is open and you add a new widget from the designer, you should regenerate code through the designer, so the files are updated to recognize the new widget you have added to your project. If the new widgets are still not recognized, try to close and reopen the project. But keep the code regeneration in mind.

I hope this helps you, and don't hesitate to ask more questions 

Mohammad MORADIST Software Developer | TouchGFX
fog.1
fog.1Author
Associate III
Jun 27, 2024 10:36 AM UTC

thank you, your suggestion worked.

ST Employee
Jun 27, 2024 12:08 PM UTC

You're very welcome!

Mohammad MORADIST Software Developer | TouchGFX