Skip to main content
LAlna.1
Associate II
May 10, 2020
Question

TouchGFX / Hardware integration tutorials

Hi there

I have been experimenting and creating simple TouchGFX GUI applications on STM32 touch screen dev kit.

Is there a simple start guide to creating as simple touchGFX GUI and controlling an LED on the STM32F429i Disco board? I tried some online examples/Youtube but they never seem to work properly.

TouchGFX websites contains good tutorials but they don't include HAL integration and control (as far as I have seen)

To keep it simple, I use ST32CubeMX, TouchGFX designer, and ST_link Utility to flash the board.

Any simple code would be a great help

Thanks

This topic has been closed for replies.

19 replies

GAuye
Associate
September 10, 2020

Update: it is not working, but I found out a "good enoght" solution.. I have started from TouchGFX, generated code, I have use .ioc in CubeMx, I have modified the file with new peripherics (GPIOs), generated code, and open all the Project in CubeIDE without modified any file name... Of course I have to live with the Project name by default (generated by TouchGFX) but at least I have full control of the Project... I'm now going to work inside the program to better understand the best and easy way to have a real application running... (it seems not so easy...) Thanks for your help!!!