Skip to main content
Associate II
Jul 7, 2025 7:31 AM UTC
Question

TouchGfx hardware acceleration libraries not included from CubeMx and CubeIde project

Hello


Project based on stm32u5g9 where I enabled TouchGfx in CubeMx settings. Layer 0 is configured to 800x600. I generate code from CubeMx. GPU2D and DMA2D are enabled and configured from CubeMx.

With TouchGfx Designer, I open the ApplicationTemplate.touchgfx.part generated or my ProjectName.touchgfx project, I see that screen dimensions are 800x480, I think it should be 800x600.

In TouchGfxDesigner, I add a screen and a box inside the screen, nothing more.

I generate code from TouchGfxDesigner.

In CubeIde, the only generated or added library I can see is :libtouchgfx-float-abi-hard.a.

I have other project generated by myself though directly from TouchGfxDesigner, chosing a STM32U5G9J-DK2 800x480 kit. Here I can see :libnemagfx-float-abi-hard.a and :libtouchgfxnema-float-abi-hard.a are included in CubeIde project.

 

In my code, I am trying to draw a scaled line, using ScalableImage, BitmapId, creating a dynamicBitmap.

Indeed the line is scaled and displayed in my display.

However the rendering time is very long, around 300 msec. I have defined RENDER_TIME_Pin, I can see the rendering time in oscilloscope.


Any help would be appreciated.


Regards.

// FrontEndApplication.cpp
static uint8_t dynamicBitmapCache[InstaScreenNamespace::kBaseWidth * InstaScreenNamespace::kBaseHeigth + 256U];

FrontendApplication::FrontendApplication(Model& m, FrontendHeap& heap)
 : FrontendApplicationBase(m, heap)
{
	Bitmap::setCache((uint16_t*)dynamicBitmapCache, sizeof(dynamicBitmapCache), 1U);
}

// InstaScreenView.hpp

class InstaScreenView : public InstaScreenViewBase
{
 touchgfx::ScalableImage scalableImageDynamic;
 BitmapId dynamicBitmapId;

 uint32_t initialcounter;
 int _line;
 int _line_1;
 int tickCounter;

 void fillDynBitMapbuffer(void);
public:
 InstaScreenView();
 virtual ~InstaScreenView() {}
 virtual void setupScreen();
 virtual void tearDownScreen();
 void handleTickEvent() override;
protected:
};

// InstaScreenView.cpp

extern "C" {extern uint8_t camera_touchgfx_started_fg;}

InstaScreenView::InstaScreenView():
		initialcounter(0),
		_line(0),
		_line_1(InstaScreenNamespace::kBaseHeigth-1),
		tickCounter(0){}

void InstaScreenView::setupScreen()
{
 dynamicBitmapId = Bitmap::dynamicBitmapCreate(InstaScreenNamespace::kBaseWidth,	InstaScreenNamespace::kBaseHeigth,
			Bitmap::BitmapFormat::ABGR2222);
 if (dynamicBitmapId != BITMAP_INVALID){
 fillDynBitMapbuffer();

 scalableImageDynamic.setBitmap(Bitmap(dynamicBitmapId));

 scalableImageDynamic.setPosition(0, 0, InstaScreenNamespace::kScaledWidth, InstaScreenNamespace::kScaledHeigth);
 scalableImageDynamic.setScalingAlgorithm(InstaScreenNamespace::kScalingAlgorithm);
 scalableImageDynamic.setVisible(true);

 add(scalableImageDynamic);
 }

 InstaScreenViewBase::setupScreen();
}

void InstaScreenView::tearDownScreen()
{
	Bitmap::clearCache();
 InstaScreenViewBase::tearDownScreen();
}

void InstaScreenView::handleTickEvent(){
	if(initialcounter < 120){
		initialcounter++;
		if(initialcounter >= 120){
			camera_touchgfx_started_fg = 1;
		}
	}
 tickCounter++;
	if (tickCounter % 2 == 0){ // Every 33 ms (2 ticks 60Hz)
		if (dynamicBitmapId != BITMAP_INVALID){
			fillDynBitMapbuffer();
			scalableImageDynamic.invalidate();
		}
	}
}

void InstaScreenView::fillDynBitMapbuffer(void){
	uint8_t* dstData = Bitmap::dynamicBitmapGetAddress(dynamicBitmapId);

	if (dstData)
	{
		Bitmap myLocalDynamicBitmap(dynamicBitmapId);
		int16_t columnNumber = myLocalDynamicBitmap.getWidth();
		int16_t lineNumber = myLocalDynamicBitmap.getHeight();
		int line;

		// Erase previous line
		line = _line_1;
		for(int16_t column = 0U; column < columnNumber; column++){
			uint32_t j = column + line * columnNumber;
			dstData[j] = 0x00;
		}

		// draw current line
		line = _line;
		for(int16_t column = 0U; column < columnNumber; column++){
			uint32_t j = column + line * columnNumber;
			dstData[j] = 0x80;
		}

		// Inc++ de la linea
		_line_1 = _line;
		_line++;
		_line %= lineNumber;
	 }
}

 

This topic has been closed for replies.

3 replies

ST Employee
Jul 7, 2025 9:06 AM UTC

Hello @rvminsta_01,

Can you provide the ioc file ?

BR,

Louis BOUDOST Software Engineer | TouchGFX
Associate II
Jul 7, 2025 9:37 AM UTC

Hello, there it is.

ST Employee
Jul 9, 2025 7:51 AM UTC

Hello @rvminsta_01 ,
It's an expected behaviour, L8 is not supported by GPU2D TouchGFX on NeoChrom/NeoChromVG | TouchGFX Documentation

BR,

Louis BOUDOST Software Engineer | TouchGFX