Skip to main content
Associate
Feb 27, 2026 10:36 PM UTC
Solved

TouchGFX hangs starting a project

I am recently retired and have used TouchGFX for my past job.  I typically run a Mac, so I decide to buy an inexpensive PC so I can do some development with TouchGFX.  I'm using a GMXtec NucBoxG3_Plus.  I've installed TouchGFX and it runs, but when I try to start a project using either the STM32F469I DISCO or the STM32H743I EVAL2, the progress bar increases to 88%, then hangs and the program exits.  I have about 400GB available on my SSD.  Any ideas?  Thanks

    ferro
    ferroBest answer
    Lead
    Mar 6, 2026 9:20 AM UTC

    ChatGPT

    The key line in your log is this:
    
    Failed to load native freetype library!
    System.IO.FileLoadException
    
    So the problem is not actually the .NET version.
    The app starts correctly, but when it loads fonts it fails to load the native FreeType library used by TouchGFX Designer.
    
    This is a native DLL dependency problem, not a managed (.NET) one.
    
    Most common cause (90% of cases)
    
    Missing Microsoft Visual C++ runtime.
    
    TouchGFX uses a native FreeType DLL compiled with MSVC, so Windows must have the Visual C++ Redistributable installed.
    
    Install both:
    
    Microsoft Visual C++ 2015–2022 Redistributable (x64)
    
    Microsoft Visual C++ 2015–2022 Redistributable (x86)
    
    Even on 64-bit Windows you usually need both.
    
    Download from Microsoft:
    https://learn.microsoft.com/en-us/cpp/windows/latest-supported-vc-redist
    
    After installing → reboot → try again.
    
    Second possible cause
    
    The FreeType DLL is missing or blocked.
    
    Check inside:
    
    C:\TouchGFX\4.26.0\designer\
    
    Look for something like:
    
    freetype.dll
    libfreetype.dll
    
    If it exists:
    
    Right-click → Properties
    
    If you see:
    
    This file came from another computer and might be blocked
    
    → click Unblock.
    
    Third possible cause
    
    Antivirus removed the DLL.
    
    Some corporate antivirus deletes unknown native DLLs.
    
    Check if the file exists in:
    
    C:\TouchGFX\4.26.0\designer
    
    If missing → reinstall TouchGFX Designer.
    
    The Windows version is fine
    
    Your log shows:
    
    Windows NT 10.0.26100.0
    
    That corresponds to Windows 11 version 24H2, which is supported.
    
    So the OS is not the issue.
    
    Quick checklist for the client machine
    
    Install
    VC++ 2015–2022 x64
    
    Install
    VC++ 2015–2022 x86
    
    Reboot
    
    If still broken → reinstall TouchGFX 4.26
    
    💡 One more thing I’d like to know
    
    Does the folder exist on his machine:
    
    C:\TouchGFX\4.26.0\designer\bin
    
    and does it contain something like:
    
    freetype.dll
    
    If you want, paste the file list from that folder and I can pinpoint the exact cause in seconds.

    4 replies

    ferro
    Lead
    Mar 3, 2026 9:23 AM UTC

    Hi @RickLeinen 

    Close GfxDesigner, delete its log file, start your project, post the log here.

    c:\Users\aa\AppData\Roaming\TouchGFX-4.26.0\TouchGFXDesigner.log

    Associate
    Mar 5, 2026 11:41 PM UTC

    Thanks for the reply ferro!

     

    I tried uninstalling and reinstalling.  No change.  I've attached the .log file.  On the TouchGFX webpage, there are two software downloads?  I downloaded both and installed the top one; X-CUBE-TOUCHGFX.  The second one will not install;

     ---------------------------
    Error
    ---------------------------
    Selected Folder does not include valid TouchGFX installation!
    ---------------------------
    OK
    ---------------------------

    ferro
    ferroBest answer
    Lead
    Mar 6, 2026 9:20 AM UTC

    ChatGPT

    The key line in your log is this:
    
    Failed to load native freetype library!
    System.IO.FileLoadException
    
    So the problem is not actually the .NET version.
    The app starts correctly, but when it loads fonts it fails to load the native FreeType library used by TouchGFX Designer.
    
    This is a native DLL dependency problem, not a managed (.NET) one.
    
    Most common cause (90% of cases)
    
    Missing Microsoft Visual C++ runtime.
    
    TouchGFX uses a native FreeType DLL compiled with MSVC, so Windows must have the Visual C++ Redistributable installed.
    
    Install both:
    
    Microsoft Visual C++ 2015–2022 Redistributable (x64)
    
    Microsoft Visual C++ 2015–2022 Redistributable (x86)
    
    Even on 64-bit Windows you usually need both.
    
    Download from Microsoft:
    https://learn.microsoft.com/en-us/cpp/windows/latest-supported-vc-redist
    
    After installing → reboot → try again.
    
    Second possible cause
    
    The FreeType DLL is missing or blocked.
    
    Check inside:
    
    C:\TouchGFX\4.26.0\designer\
    
    Look for something like:
    
    freetype.dll
    libfreetype.dll
    
    If it exists:
    
    Right-click → Properties
    
    If you see:
    
    This file came from another computer and might be blocked
    
    → click Unblock.
    
    Third possible cause
    
    Antivirus removed the DLL.
    
    Some corporate antivirus deletes unknown native DLLs.
    
    Check if the file exists in:
    
    C:\TouchGFX\4.26.0\designer
    
    If missing → reinstall TouchGFX Designer.
    
    The Windows version is fine
    
    Your log shows:
    
    Windows NT 10.0.26100.0
    
    That corresponds to Windows 11 version 24H2, which is supported.
    
    So the OS is not the issue.
    
    Quick checklist for the client machine
    
    Install
    VC++ 2015–2022 x64
    
    Install
    VC++ 2015–2022 x86
    
    Reboot
    
    If still broken → reinstall TouchGFX 4.26
    
    💡 One more thing I’d like to know
    
    Does the folder exist on his machine:
    
    C:\TouchGFX\4.26.0\designer\bin
    
    and does it contain something like:
    
    freetype.dll
    
    If you want, paste the file list from that folder and I can pinpoint the exact cause in seconds.